Component | Quantity | |
Battery | Li-ion Battery 3.7V 1300mAh LB-040 | 1 |
* Battery charger (LBB-040) sold separately
Detach the battery from the robot or controller when storing away.
When storing away the battery for a long time, make sure the battery life is around 50%.
※ Li-ion Battery 3.7V 1300mAh LB-040 has a warranty period of 6 months.
Controller : CM-150, OpenCM9.04
Battery Charger : Li-ion Battery Charger Set LBB-040
This battery can NOT be connected directly to the controller. You will need the Li-ion Battery Charger Set LBB-040 to connect to the controller (robot).
Do not drop or give impact.
Do not operate while charging.
Do not apply heat, water or any other liquid on the battery.
Do not place in the microwave, washing machine or dryer.
Do not use damaged batteries (inflated, deformed, damaged, etc.).
Do not short circuit the polarity.
Do not take the battery apart.
When charging, make sure the battery is connected into the correct polarity.
Do not charge when the battery is hot. Please charge after it has cooled off.
Do not keep the battery connected to the controller when not in use.