Features

Gripper frame set for DYNAMIXEL X430 series.

Can be used with XH/XM430 or XL430, XC430 depending on the idler set.

Package Components
FR12-E170GM1
FR12-E171GM1
WB M2x312
FHS M2.5x146
Spacer Ring6

*Idler set not included in package. 

Compatible Products

Dynamixel X430 series (all models)

Please refer to the compatibility chart for more information.


Caution

Idler set is required to use this frame with DYNAMIXEL X430.

Be sure to purchase one of the idler sets below.

 

XH430, XM430 : HN12-I101 Set

XL430, XC430 : HN11-I101 Set