Features

Hinge frame set for DYNAMIXEL X430 series.

Same frame used on the lower part of the ROBOTIS OP3.


Package Components
FR12-H103GM1
WB M2x4K10
WB M2.5x48

*Idler set not included in package. 

Compatible Products

Can be used with XH/XM430 or XL430, XC430 depending on the idler set.

Dynamixel X430 series (all models)

Please refer to the compatibility chart for more information.


Caution

Idler set is required to use this frame with DYNAMIXEL X430.

Be sure to purchase one of the idler sets below.

 

XH430, XM430 : HN12-I101 Set

XL430, XC430 : HN11-I101 Set